AXIS#.HOME.OFFSETUSER

Description

This keyword allows the user to add an offset to the feedback after homing has been completed. This is intended to be used to compensate for home switches which may not be perfectly placed or misaligned with a gantry axis.


  • This keyword can be set before or after homing has been completed but WILL NOT be used until homing is complete. If homing is re-issued, this compensation is removed during homing and then re-applied after homing has been completed.

  • Once homing has been completed, this value takes effect immediately. If the axis is enabled, the axis will jump by the same amount this keyword changes as an instantaneous offset. Care should be taken when modifying this value. It is not intended to be used with large changes.

  • Once homing has been completed, this value takes effect immediately. If the axis is enabled, the axis will jump within a few milliseconds to make up the difference (e.g. from 5 to 10 will jump 5 units). Care should be taken when modifying this value as it is not intended to be used with large changes.

Versions

Action Version Notes
Implemented 02-03-04-000  

General Information

Type Read/Write
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value

N/A

Data Type Float
See Also AXIS#.HOME.OFFSETUSERLIMIT
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
AXIS1.HOME.OFFSETUSER

5008h

0eh

Signed32

Position

-

Read/Write

No

AXIS2.HOME.OFFSETUSER

5108h

0eh

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.OFFSETUSER

6117

17E5

Signed32

Read/Write

Position

AXIS2.HOME.OFFSETUSER

71653

117E

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.OFFSETUSER

6117

Signed32

Read/Write

Position